Other Parts Discussed in Thread: ADS1018
The power is using 5V, we use single-ended inputs, in datasheet of ADS1018-Q1,the FSR can be configured as ±6.144V, ±4.096V, ±2.048V, ±1.024V, ±0.512V, ±0.256V, what the sourcing of FSR,why it can exceed the power supply voltage and What is the maximum voltage value that can be input?