请问我的代码由什么问题吗?我读取不到ADC 0123通道的值。
已经通过示波器查看SPI接口 Data changed on SCK 1st edge, captured on 2nd , SCK Signal is Active Low (idles high).
感觉SPI通讯时序没有错误,就是读出来的ADC值始终是32772不会改变
初始化代码:
void InitTLC3544 (void){
ADC_CSN(0);
SPI2_ReadWrite(0xA000,RW_16_Bit);
ADC_CSN(1);
Delay_ms(10);
ADC_CSN(0);
SPI2_ReadWrite(0xA800,RW_16_Bit);
ADC_CSN(1);
Delay_ms(10);
}
读取ADC通道值代码:
Read_Once_TLC3544 (void){
ADC_CSN(0);
print("\r\n 0ch = %d",SPI2_ReadWrite(0x0000,RW_16_Bit));
ADC_CSN(1);
Delay_ms(100);
ADC_CSN(0);
print("\r\n 1ch = %d",SPI2_ReadWrite(0x1000,RW_16_Bit));
ADC_CSN(1);
Delay_ms(100);
ADC_CSN(0);
print("\r\n 2ch = %d",SPI2_ReadWrite(0x2000,RW_16_Bit));
ADC_CSN(1);
Delay_ms(100);
ADC_CSN(0);
print("\r\n 3ch = %d",SPI2_ReadWrite(0x3000,RW_16_Bit));
ADC_CSN(1);
Delay_ms(100);
}