This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1259: AMC1301输出能否与ADS1259直接连接?

Part Number: ADS1259
Other Parts Discussed in Thread: AMC1301,

  • 您好,

    在您的应用中,AMC1301输出范围是多少?请注意AMC1301有1.44V左右的共模电压。

    ADS1259使用的是内部基准电压还是外部基准电压?若是外部,使用的是几伏?

  • AMC1301差分输出范围是0~2V,共模电压是1.44V,相当于VOP是1.44V~3.44V,VON是1.44V(我理解是这样的),ADS1259是单+5V供电,使用外部基准,基准电压是2.5V,不知道是否能够直接连接,若不能需要如何使用

  • ADS1259差分输入范围是±VREF,如VREF=2.5V,则ADS1259差分输入范围是±2.5V,是可以满足AMC1301的0~2V差分输出的

    ADS1259的单端输入范围是AVSS-0.1V ~ AVDD+0.1V,若ADS1259是单+5V供电的话,则为-0.1V ~ 5.1V,也可以满足VOP(1.44V~3.44V)和VON(1.44V)的要求的