This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1298 I/O口电平

Other Parts Discussed in Thread: ADS1298

1. 如果ADS1298采用3.3V模拟电源供应,1.8V数字电源供应,其SPI端口和其他数字端口的电平是3.3V的电平么? 

2. 若ADS1298只作为一般的模数转换作用,不用于ECG,芯片的特殊功能如RLD、LEAD-OFF DETECTION、WCT、PACE -DETECTION 都是用不到的?

3. ADS对微处理器有什么特别要求?能否不用DSP处理器,而用STC系列的8位单片机如STC12LE60S2控制或者其他的如ARM?

 

  • 3.3V 模拟电源是给模拟信号供电的,1.8V数字电源是给数字信号供电的,像SPI接口和其他数字端口的电平都是1.8V的。

  • 1. 数字端口电平又数字电源提供,所以SPI端口和其他数字端口电平为1.8V。

    2. ADS1298是专门用于做心电信号采集的模拟前端,如果只用作模数转换作用,就失去了其价值所在。可否请楼主描述一下应用领域?

    3. ADS1298对心电信号采集之后设计心电信号的算法处理,而DSP在处理复杂算法方面优势明显,所以还是建议采用DSP做信号处理,可以评估一下TMS320C5000系列DSP。而对于系统的控制方面,楼主可以评估TI的Sitara AM335X或者AM18X系列处理器。

    希望能够帮到您!

  • 用于环境磁场信号检测,需要一个精度比较高而且能够实现同步采样的ADC,于是参考了下ADS1298这款芯片。不知ADS1298的相对精度如何,资料中只给出了测试信号(1mv、2mv)的精度,若输入端输入一个1V的信号,输出端的误差会有多大呢?