This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC38RF85: 器件RF信号无输出

Part Number: DAC38RF85


Ti工程师您好!

我们正在使用DAC38RF85以及zynq7045进行调试。尝试发1900MHz信号,LMFSHd=22210。

时钟方面,使用内部PLL模式,输入时钟2200MHz,内部PLL锁定5500MHz,目前已能在CLK_TX端口上量到其4分频的时钟频率1375MHz,证明PLL工作正常。

204B接口方面,目前通过Vivado ILA监测sync信号,接口建链正常。(CGS和ILAS阶段已通过,sync变为高电平)

目前通过配置0x12F和0x130寄存器能发出单音信号,关闭SPIDAC测试模式后,DAC就无输出了。目前已将所有告警寄存器mask,以及关闭了所有可能清零JESD block输出数据的寄存器。但仍然无法在频谱仪上看到一点点波形。烦请TI工程师帮忙解答一下