This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE4403: OSC 電壓不同,可否正常工作

Part Number: AFE4403

AFE4403 3.3V供電、使用 µPower Oscillator 3.3V  8MHz XIN。目前想把 OSC 移除,改用 MCU 產生  8MHz  輸入到 AFE 的 XIN。

可 MCU 1.8V 供電,   AFE4403  XIN 電壓 1.8V 可以正常使用嗎?

  • 您好,XIN参考的是RX_DIG_SUP的电压,而RX_DIG_SUP的电压范围为2.0~3.6V之间,所以如果RX_DIG_SUP=3.3V的话,XIN的Vih(min)=0.75*3.3=2.475V。所以1.8V是不允许的,可以考虑加一颗1.8V到3.3V的电平转换芯片。