Other Parts Discussed in Thread: DAC161S997, DAC161S997EVM
尊敬的工程师您好,我在DAC8742H数据手册中发现,HART通信时Receiver sensitivity是80-120mvpp,这个意思是指当信号电压值讲到此范围以下时,此信号不被接收吗?还是说会带来其他的结果?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
尊敬的工程师您好,我在DAC8742H数据手册中发现,HART通信时Receiver sensitivity是80-120mvpp,这个意思是指当信号电压值讲到此范围以下时,此信号不被接收吗?还是说会带来其他的结果?
您好,这里的意思是,MOD_IN的幅值在80~120mv之间时,检测到有效载波信号,CD拉高并且开始进行解调。 如果不在这个范围内,比如低于80mV或者高于120mV,CD拉低,检测不到载波信号,所以这个Receiver sensitivity指的是在HART mode下,载波检测的阈值电压范围。
您好,关于这个问题我还想继续跟您探讨一下,我首先想确认这个80mV和120mV是经过DAC8742H 的HART内置解调带通滤波器之前的值吗?为什么他会有80-120这样的一个波动呢?实际的HART信号到MOD-IN管脚时候的范围是多少,是80-120mV吗?第二:这个幅值范围对应的频率是多少,换句话说,如果有一个不是1.2K或者2.2K的其他频率噪声信号,这个幅值应该降到多少才能保证这个信号的取值不会影响到HART信号的解调?第三个问题是我将DAC8742H与DAC161S997连接以后,我发现解调信号在进入HART带通滤波器之前,会首先经过一个RC网络,比如下面的截图是在DAC161S997EVM里面截取的部分,这个网络的目的是对HART信号进行衰减吗?意思是将一个500mV左右的HART信号衰减成一个80-120mV的信号吗?如果是这样,为什么这个网络会具有衰减作用呢?非常感谢您,我很困惑,期待您的专业解答。