DAC8563xa中的10脚原本是输出2.5v电压,现在有时候有输出2.5v,有时候没有,是不是基本上能确定是芯片坏了
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这个板子换了其他可以正常工作的DAC8563芯片后,这个板子正常工作了吗?如果正常工作了,可能是DAC8563芯片的问题;
从这个板子拆下来,换在其他可以正常工作的板子上,正常的板子还能正常工作吗?如果还可以正常工作,那么就是焊接的问题,若不能工作就是这个芯片的问题
抱歉,另外请再确认下,是否使用DAC8563的VREF给其他负载供电了?外接电路是否按datasheet典型电路接的?
因为如果从TI正规渠道购买的产品的话,一般是没有问题的,所以判断是否异常需考虑各方面原因
我又看了下DAC8563 datasheet,其内部基准默认是disable的,并且The internal reference is forced to a powered-down state while both DAC channels are powered down, and is only enabled if any DAC channel is also in the normal mode of operation
所以还请确认是否因发送了一些命令导致内部VREF有时有输出,有时没有