Part Number: ADS125H01
使用ADS125H01进行电压检测,参考电压为5V,PGA设置为0.5,设计输入范围为±10V。
在低压(小于2V)的输入时,结果比较正常,仅仅稍有波动。
当输入超过3V时,结果会在两个数值之间跳变,两个数值的差别大约在0.017V,远远大于低压时的数据波动幅度,每次结果值跳变大约会持续10s以上。
请问这是什么原因导致的数值跳变,如何规避此类问题?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.