1、AFE5816 采集不到信号波形?在设计中,我配置AEF5816为TGC模式,外部Rs选择为50欧姆,固定增益模式,40Mz采样。在测试过程中,FPGA已经能够收到正确的测试码,但是,无论我把增益调到多大,FPGA始终不能看到信号波形。
2、AFE5816能够能够失能衰减器吗?


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1、AFE5816 采集不到信号波形?在设计中,我配置AEF5816为TGC模式,外部Rs选择为50欧姆,固定增益模式,40Mz采样。在测试过程中,FPGA已经能够收到正确的测试码,但是,无论我把增益调到多大,FPGA始终不能看到信号波形。
2、AFE5816能够能够失能衰减器吗?


外部Rs选择为50欧姆,但是您在输入处添加了分压电路,即R2614和R2526 或R2615和R2550,那么其信号源阻抗就不再是50Ω了,它应该是相当于(RS+R2614)//R2526 ;
再看9.3.3 High-Pass Filter (HPF),e LNA High-Pass Filter (LNA HPF)这个滤波器没问题, Attenuator High-Pass Filter (ATTEN HPF)这个滤波器还需要公式3计算下高通滤波器的截至频率:

这个LNA_INCM引脚电压正常应该是1V,因此直流耦合输入的话,您还需设置偏置电压到1V
刚注意到,您将INM接地了,INM不可以直接接地的,看注释(3)
AFE5816 datasheet没有说可以直流耦合,但我认为设置好合适的直流偏置,应该是可以的