This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8328: 多通道AD通道串扰

Part Number: ADS8328


ADS8328两个通道分别采样两个电压,以200k的速度轮流以采V1,V2经对比发现,只采V1或者V2采样非常稳定,轮流采样时波动会有40mV左右。怀疑是ADS8328本身串扰了。请问如何解决。

  • 您好,

    您可以用示波器实测ADS8328两通道的模拟输入端,对比看是不是在模拟信号输入至ADS8328前就已经串扰了?如果是的话,那就需要在PCB布局上去解决

  • 0到80V采样波动40mV左右,示波器应该测不出来。应该不是板上的问题,因为单独采V1或者 V2时其实两个通道都已经在板上了,信号已经到了ADS8328端口,只是没采样。单独采的跟两路同时采的波动幅度不一样,单独采V1或者V2波动幅度10mV左右,同时采波动40mV左右。

  • 我调节了下前级滤波参数,但是两个通道轮流采还是稍差一点。波动范围会多5个mV。考虑到采样范围0到80V,已经基本能接受了。如果到时候测不过就换成两片ads8237。请教下这种互相影响到底是正常现象还是我板子的问题。

  • 我不知道您是怎样实现的0到80V采样,因为ADS8328模拟输入范围没有这么大;另外,为什么您调节前级滤波参数,两个通道轮流采时波动幅值缩小了呢?是否与您的前级滤波电路有关呢?