This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1291: 输出波形错误

Part Number: ADS1291
Other Parts Discussed in Thread: ADS1292R, ADS1292, ADS1192

我们在开发一个带ECG功能的手环,选了TI的ADS1291芯片,现在发现ECG的波形没有出来,感觉都是杂波,我们现在只有2个电极,一个接左手(LEFT)一个接右手(RIGHT),请帮忙看看电路图和寄存器配置有没有问题,谢谢。

  • 您好,

    ADS1291 , ADS1292 和 ADS1292R 都采用相同的封装 / 引脚输出,ADS1291只有一个模拟输入通道,ADS1192有2个,后缀带R的ADS1292R具有呼吸(respiration )功能。IN2N, IN2P,RESP_MODN,RESP_MODP这些不用的管脚可以上拉至AVDD。另外实测检查下基准电压正确吗

  • 1,我们量了基准电压是2.424V,不知道这个有没有问题?
    2,上次我发给您的电路原理图有没有问题?
    3,还有就是我们的寄存器配置有没有问题?
     
    #define ADS1291_2_REGDEFAULT_CONFIG1 0x00 //00/< Continuous conversion, data rate 
    #define ADS1291_2_REGDEFAULT_CONFIG2 0xA0 //A3/< LOFF off, REFBUF on, VREF=2.42, CLK_EN=0, INT_TEST=1, TEST_FREQ @ 1Hz
    #define ADS1291_2_REGDEFAULT_LOFF 0x00 //00/< 95%/5% LOFF comparator threshold, DC lead-off at 6 nA
    #define ADS1291_2_REGDEFAULT_CH1SET 0x60      //0x60 ///< Channel on, G=12, normal electrode
    #define ADS1291_2_REGDEFAULT_CH2SET 0x91 //91/< Channel off, G=1, input short
    #define ADS1291_2_REGDEFAULT_RLD_SENS  0x00 //23/< Chop @ fmod/16, RLD buffer on, LOFF off, RLD derivation from CH1 P+N
    #define ADS1291_2_REGDEFAULT_LOFF_SENS 0x00 //00/< Current source @ IN+, sink @ IN-, all LOFF channels disconnected
    #define ADS1291_2_REGDEFAULT_LOFF_STAT 0x1f //00/< Fmod = fclk/4 (for fclk = 512 kHz)
    #define ADS1291_2_REGDEFAULT_RESP1 0x02 //02/< Resp measurement disabled
    #define ADS1291_2_REGDEFAULT_RESP2 0x07 //07/< Offset calibration disabled, RLD internally generated
    #define ADS1291_2_REGDEFAULT_GPIO 0x00 //00/< All GPIO set to output, logic low
  • 您好,测量了基准电压是2.424V,想问一下原理图和寄存器配置是否正常,我们用的是1291?

  • 基准电压使用的是内部基准2.42V,电压值是正确的;

    ADS1291只有一个模拟输入通道,是IN1N和IN1P,其他的IN2N, IN2P,RESP_MODN,RESP_MODP,ADS1291都是没有这些功能的;

    因为接入人体信号操作不当,很容易引入干扰信号,因此建议先输入ECG模拟仪的信号验证电路

  • 请问一下,我们的基准电压用示波器测量发现他一直在 2.45   2.46   2.47  这3个值跳动,这个是什么原因,要从哪方面检查?

  • 我在您给的电路图中,看到有2种类型的地,不知道这两种地是否短接在一起了?VREFN是需要和AVSS连接在一起的

    您用示波器实测AVDD是稳定的吗