This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1263: 这个32位的AD直接连接电桥是否有好的测量精度

Part Number: ADS1263
Other Parts Discussed in Thread: INA128, ADS1255, ADS1262

尊敬的工程师:

您好,Datasheet中,ADS1263在首页的图中就直接连接了电桥进行测量,如下图所示:

我们公司以前都是采用仪表放大器+24位AD(例如INA128仪表放大器 + ADS1255)进行产品的设计,采集的精度还是不错的.

这次我们正在使用ADS1263进行设计,根据手册中的参数,它的PGA只有32,对于一般电桥输出的满量程电压正负20mv,那么放大后的电压也只有正负0.64V。

我们看到手册上直接连接电桥的微弱信号,我是不是可以理解为这种32bit的AD就不需要使用仪表放大器作为前级也能保证我们以前的精度,不知道这样理解对吗?

非常感谢!

祝您好心情!