我的顺序是上电,然后发送复位命令,延时一段时间,接着发送0x47,在发送0x02。无法启用内部温度传感器模式。
然后在读取寄存器时,发送0x27,意思是读取寄存器1的4个字节,然后给ADS1220器件8个始终来读取寄存器1的配置(比如发送的0x55),也无法读得寄存器1的配置,收到的是0xff。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我的顺序是上电,然后发送复位命令,延时一段时间,接着发送0x47,在发送0x02。无法启用内部温度传感器模式。
然后在读取寄存器时,发送0x27,意思是读取寄存器1的4个字节,然后给ADS1220器件8个始终来读取寄存器1的配置(比如发送的0x55),也无法读得寄存器1的配置,收到的是0xff。
您好,
读写寄存器命令中的rr是要读写的多个寄存器中的第一个寄存器的地址,nn是要读写的寄存器个数-1。如果您要写一个寄存器值,那么nn就是00,地址rr就是这个寄存器的地址。发送0100rr11意思是对4个寄存器进行写操作,ADS1220只有4个寄存器,那么需要从第一个寄存器开始写才能写入4个值,第一个寄存器的地址是00,那么rr就是00,因此需要发送命令01000011,也就是0x43,而不是0x47,然后在发送要写的4个寄存器值;
如果您只对01h寄存器写入0x02,那么需要发送的命令是01000100,即0x44
读是一样的,仅是命令不同