对于ADS1299的裸芯片而言,怎么测试他是否能正常工作,直接给他上电看电流值是否可以。
目前我将ADS1299的所有引脚引出,并连上AVDD(5V),AVSS(0V),AGND(0V),DVDD(1.8V)(其他都没有连接),DVDD没有电流,看到AVDD的电流波动很大,这是否说明芯片有问题?还是要连上VCAP,晶振等引脚才能看出芯片是否工作在正常情况下。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
对于ADS1299的裸芯片而言,怎么测试他是否能正常工作,直接给他上电看电流值是否可以。
目前我将ADS1299的所有引脚引出,并连上AVDD(5V),AVSS(0V),AGND(0V),DVDD(1.8V)(其他都没有连接),DVDD没有电流,看到AVDD的电流波动很大,这是否说明芯片有问题?还是要连上VCAP,晶振等引脚才能看出芯片是否工作在正常情况下。
您好,
如果仅看ADS1299的各供电或者说消耗的功率,我认为这不能完全确认ADS1299是否正常,供电电压正常是判断ADS1299是否正常的其中的一个必须的步骤;
如果不能将芯片焊接在电路板上的话,我认为需要做一个工装板,将ADS1299各管脚引出来,在工装板上搭建您需要的功能电路,在工装板上验证您需要的功能是否正常工作。这里需要想办法将裸芯片的各管脚与工装板上的ADS1299 PCB封装的各管脚连接导通。
下面FAQ说明了验证 ADS129x 器件是否仍然正常工作的步骤: