Part Number: DAC8760
Other Parts Discussed in Thread: DAC8750,
1,芯片容易坏,现象是IOUT输出容易变0mA,而不是默认的4mA;只能通过替换芯片方式解决。
2,IOUT 是否可以串接个 二极管 输出 ?
麻烦您看看原理图,是不是原理图有问题,或者外围元件不适配。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1、AVDD、AVSS供电是多少?使用内部DVDD供电的话,DVDD最多只能输出10mA,请确认外接3个AUDM3201所需电流在这个范围内
您可以给出上面这一点的情况吗?
因为D9 TVS管是用的±15V的,但是您“8760默认配置完正常的花IOUT电压表量会有24V电压”,这已经超过了您使用的TVS管