This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC7836: AMC7836的ADC端口和LV_ADC端口不用应该怎么接

Part Number: AMC7836

芯片手册上说ADC和LV_ADC是用来监测DAC输出的。请问

(1)如果我不使用这个监测功能DAC能正常工作吗?

(2)不用这些AD输入口的话,电路应该怎么接呢,悬空or上下拉?

  • 您好,

    AMC7836的ADC可以不用来检测DAC输出,也可以用作普通的ADC采集

    1、不使用这个监测功能DAC能正常工作

    2、一般输入接口都不可以悬空的,不使用的ADC输入可以直接接地;如果您仅使用DAC功能,您可以选择其他的DAC专用芯片,避免AMC7836的ADC资源浪费