Other Parts Discussed in Thread: OPA140,
如果我的基准输入最大4.65V(OPA140缓冲,电源电压±5V),实际输入信号最大只有40mV,那么我的积分电阻器的值该怎么计算?参照手册上的
计算结果不好用,测试不对。如果给100K,就符合应用。
另外,没想明白这个第一阶段的自动归零是怎么实现的,按照内部电路结构,闭合对应开关,没想出来怎么工作的,这个是否可以解答下,理解清楚了,后面3个阶段才好理解。闭合开关后,如下图右上角所示,对吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
OPA140那个我清楚,是缓冲过来的,反相跨阻接法,同相端为地,输出是可以达到4.65V的。
主要就是那个积分电阻,datasheet说的是输入除以积分电流,貌似和基准电压无关,实际似乎不是这样。
应用时那个A/Z过程没看懂电路原理,所以分清楚积分电阻到底怎么算。
这个是比较老的器件了,除了datasheet我没找到关于它的其他资料
您使用的供电电压是多少?根据datasheet ,Vref应该在正负供电电压之间,典型值为1V
如果您使用±5V供电的话,Vref=4.65V是满足要求的,Full Scale Voltage应该为2*Vref=9.3V,根据RINT的计算公式,选择IINT=20uA,可以计算出RINT=465K;
如果实际输入信号最大只有40mV,建议使用datasheet推荐的Vref=1V,这样RINT=100K