AVDD、DVDD接3.3V供电,想要REFOUT输出2.5V供外部传感器使用。REFOUT与REFCOM之间接1uf电容时输出为0V,电流很大,约90mA,REFOUT与REFCOM之间不接1uf电容时输出为1.81V,电流正常,怎么回事?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
下面表格是datasheet截图,ADS124S06在3.3V供电时,其输出电流大概约5mA,短路电流典型值为70mA
您连接外部传感器时,是否对地短路了,使得电流为90mA?
REFOUT与REFCOM之间最小电容是1uF,不可以不接电容,不接电容可能工作异常:
REFOUT与REFCOM之间不接1uf电容时输出为1.81V,电流正常
您外接的传感器所需最大电流是多少?

直流电源显示的AD+主控的电流在3mA
您可以详细说明一下,您测电流的接线方式吗?AD+是什么?REFOUT作为输出,您使用的负载是什么呢?有负载才能构成回路,才能有电流输出
没发现哪里的软件配置或电容配置会导致内部基准短路
您是在TI.com官网购买的ADS124S06吗,如果不是,请与供货商确认产品的最终购货来源为TI。另外,您使用的具体型号是什么呢,在下面产品首页,如下图所示,下面两种型号可以申请样片,如果型号与这两种一致,建议申请样片试一下,看是否为产品本身问题