请问专家怎么回事?我把电路板的地直接接到AD1258的输入端,读出来的数不是0,是10.66V这个电压是我根据datasheet里的公式计算出来的,AVDD接5V,AVSS接地。ADS1258和电路板是共地的,是否会是这个芯片坏了呢?但是在有电压输入的时候,比如输入到AD的电压为2.5V的时候,就能正常转换出来,这是为什么呢?而且我这里有2块一模一样的电路板,一块是好的,完全正常,而另一块就是我上面说的情况。有问题的这块电路板上的ADS1258已经更换过一块新的了,问题还是存在,晶振也换了,求专家指导啊。还有就是如果AD的输入超过了AVSS-100mv,那AD转换出来的数是多少呢?