This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1224 模数转换问题

Other Parts Discussed in Thread: ADS1224

使用ADS1224,将四个输入的正向输入和反向输入都接地,此时转换后的数字信号应为0V,可为什么显示的结果是9mV?

  • ADS1224是24位DM-ADC,其分辨率决定了对噪声的敏感性。您的接地要保证绝对干净,一旦有超过1/2LSBde 噪声通过地线输入ADC,就会对ADC的输出造成影响。请先确定9mV是否为噪声,另外显示结果是9mV固定不变还是不停跳变?请楼主提供详细的测试条件,谢谢!

  • 接地接电源电,电路板上所有元器件供用的地,9mV是固定不变的。

    如果正向输入不接地,接信号的话,输出值为信号电压值加9mV.

  • 你使用了内部的buffer 了嘛,如果打开了buffer。绝对的电压输入范围是不能到地的。为GND + 0.05V到 AVDD − 1.5V。

    一般测试的ADC的offset是将ADC在内部短接或引脚处短接。并接到一个低噪基准源上测试。

    你在ADC的引脚处,用万精度的万用表。测一下差分电压值