This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
这很可能是输入端悬空造成的,一般不管是模拟输入端还是数字输入端都是不能悬空的,您将输入端接有效输入信号,OTRA/OTRD是否可以正确指示状态?
您是参考ADS1675 datasheet中Figure 55 使用THS4503实现单端转差分信号吗?如下截图,
您问的是下图红色圈内 CM 2.5V的作用是吗?这个图使用的不是对称电源,其中间电压值是2.5V,将输入基准设为2.5V应该是为了有最大的信号输入范围
请给出以下信息:
1、您是使用THS4503实现单端转差分信号吗?然后THS4503输出接ADS1675?
2、ADS1675的基准电压是多少?
3、上面的3.8V是指的ADS1675的差分输入电压吗?
4、您可以附上THS4503+ADS1675相关电路吗?
我看电路图中THS4503被R19和R29短接了,您实际应用中是不是也是被短接的?
ADS1675需要有2.5V的共模输入电压,其差分输入范围是±VREF ,在您的应用中也就是±3V,因此,如果ADS1675的输入电压是差分的3.8V,那么模拟输入就超出了ADS1675的输入范围
这个输入至ADS1675的3.8V电压是什么电压? 您是怎样测量出来的?
在您的这个电路中将THS4503的VOCM这个引脚给上了1.2V的电压,ADS1675是否正常?
THS4503的共模电压为2.5V,ADS1675的基准电压为3V,这2点并不能说明ADS1675的输入信号在其正常范围内;
您可以用示波器测量ADS1675的AINP对地电压波形、AINN对地电压波形和AINP-AINN的差分电压波形吗?建议将前面2个的单端波形显示在同一示波器界面中