This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC12DJ3200: jesd204b 接口资讯

Part Number: ADC12DJ3200


1. 使用该芯片jmode0  模式发送数据,最大速率是单通道12.8G,利用的是通道da0-3和db0-3  8个通道,想咨询下通道a和通道b两组通道在布线时是否需要做通道信号延迟补偿(jmode0 模式 8个通道等长拉至接收端还是需要补偿每个通道间的延迟,还是松散等长没有严格等长要求),我发现手册也没有提通道间延迟这个参数,不需要补偿么?完全靠接收端伸缩buffer硬收?这块是什么建议

  • 您好,没有找到相关应用手册说明,但依我个人的经验,两个通道间的差分数据线的布线尽量等长等间距,长度尽量控制在5mil之内。 

  • 我把这个通道延迟描述细点,一般芯片die是通过基板和bga锡球连到电路板上,那么每个收发器通道间从die到基板传输可能存在走线不等的误差,导致走线延时不一致,我们对端FPGA在做ddr时指出在高速时必须补偿这个管脚间延迟。而对于204B收发器接口,FPGA端咨询过是不需要考虑这个延迟补偿的。不过adc这边是2组204b接口,两组204b接口之间是否会存在这个延迟补偿问题,还是说忽略这部分

  • 对于da0-3和db0-3  8个通道,走线不等的误差尽量控制在5mil之内,如果误差太大就会引起信号完整性的问题了。

    对于ADC12DJ3200的走线要求,需要按照datasheet中10.1 Layout Guidelines的规则,参考Figure 194的top层的布线。 

    datasheet中也没有提到补偿问题。

    所以我的建议是按照datasheet中的guidelines布线,对于这几个通道的data来说,等间距是能做到的,等长尽量控制在5mil之内,不会有太大误差。