This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8661: ADS8661寄存器如何配置可使alarm输出报警

Part Number: ADS8661


我们现在使用ADS8661数模转换器,采样数据读取正常,我们打算使用ads8661的input alarm功能在电压超门限的时候产生报警信号,我配置了下面的寄存器:

1.  地址14寄存器RANGE_SEL_REG配置为0x000b

2. 地址0c寄存器SDO_CTL_REG配置为0x0100

3.地址24寄存器ALARM_H_TH_REG配置为0xc800

但是alarm信号在电压超过门限后并不会自动拉高,我想请教一下谁用过相关功能吗?寄存器该如何设置?

另外还有一个现象就是如果上电单纯配置上面几个寄存器,alarm信号并不会置低,上电后先复位一下再配置才会置低,但是读采样数据功能并不需要复位,想问一下上电复位是必须的步骤吗?

谢谢!