This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS1209 - SYNC输出与TestMode

1、在TestMode下,为什么有SYNC输出?而且输出频率与CONV_CLK频率不相关。CONV_CLK为100kHZ,SYNC输出为3MHz或者6.8MHz左右,不固定。即使CONV_CLK信号停止了,仍然有SYNC输出。

2、读数据的过程中,/RD信号为由CONV_CLK经过延时产生。/RD低电平的半周期内,数据线上的数据不是稳定的,而是有几次方波样的跳变。

3、在TestMode下,Control Register0的bit7-3的设定是否可以为任意值?

盼回复!