Other Parts Discussed in Thread: ADS54J69, ADS54J40, ADS54J66
你好,我想用我的电脑配置ADS54j69evm,已经装有软件ADS54Jxx EVM GUI V1.8,但是该软件里面并没有可供选择的器件,是否能配置?如果不能,还请指导一下。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,ADS54Jxx系列中的所有器件,包括ADS54J69,都将在GUI窗口中显示为ADS54J40.所以这里可以选择为ADS54J40。 参考下面类似的帖子,里面有详细的解释:
All parts in the ADS54Jxx family, including the ADS54J66, will show up as an ADS54J40 in the GUI window. They all have the same SPI interface and you can program all of them with any file the GUI comes with. But, some of these file will not work. It is up to the user to follow the User's Guide and only load the files called out or the ones with the part name in the configuration file. In your case, you can use any file that starts with 'ADS5xJx_" or the one called "ADS54J66_bypass_4211.
It make sense!
Thank you.