你好
我需要得到50或60个方波电压且赋值可调,之前用的是4xDAC61416,现在想用DAC60096,我想问一下,它们之间有什么比较明显的区别吗?有无输出缓冲会对负载有什么影响?
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好
我需要得到50或60个方波电压且赋值可调,之前用的是4xDAC61416,现在想用DAC60096,我想问一下,它们之间有什么比较明显的区别吗?有无输出缓冲会对负载有什么影响?
谢谢
DAC60096输出缓冲器的选择需配合具体应用选择,DAC输出电压的话,需要考虑使用高输入阻抗、低输出阻抗的运放,然后就是运放增加的settling time 、SR、输出电压范围等
查看两个芯片的规格书后,发现输出阻抗分别维40Ω和41KΩ,考虑到我这边需要的是电压,能不能帮忙推荐适合DAC60096的缓冲器芯片?通道数量最少60CH
抱歉,我们没有60CH的运放,最多的通道数是4,因此,需要使用15 pcs才能可以,我不知道您那边是否考虑使用15pcs x 4 channels 运放的方案?如果可以的话,我再给您推荐
是的,DAC60096输出阻抗与外接负载是串联的,DAC60096输出阻抗越高,信号源电压降落在了自身内阻上的就越多,对外界提供的信号幅值影响就越大
(就越低)。