This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS54J60: 模拟输入端对地阻抗近乎于0

Part Number: ADS54J60


我们设计的每块PCB有两片ADS54J60IRMP 1GSPS,双通道。我们的PCB经过测试,功能均正常。

最近,有一块PCB中的两片ADS54J60芯片只有一个通道能正常使用,另一个通道则一直采集噪声如下图。同样的程序,其他PCB双通道正常。

经过排查,断开前端输入,对比两片ADC芯片:

ADC1:测量模拟输入端口INA_P/N,对地阻抗均为1.2KΩ,该通道是功能正常的;

          而测量INB_P/N对地阻抗均接近0Ω,该通道是不正常的;

ADC2:INA_P对地阻抗为1.2KΩ,INA_N对地阻抗均为20Ω,该通道是功能不正常的;

          而测量INB_P/N对地阻抗均为1.2KΩ,该通道是功能正常的。

我们其他的PCB没有发现这个问题,为避免以后出现这个问题,特来询问这会是什么原因造成的呢?这是否就代表ADC已经损坏呢? 前端电路如下。