我在使用ads1292R这款IC的时候,根据其spec,在遵守spi总线协议的前提下,各项寄存器配置均已配置ok(读回来的值和写入值一致),使用的是内部时钟512khz(可以测量到),内部参考电压(2.42V,可以测量到),使能内部测试信号(1mv,1Hz),连续采集模式,DRDY信号正常(125sps),但是测试信号转换后的结果,无法确认其正确性,PGA增益设为6(默认值)的前提下,测试信号的结果约为0x001104E1(十进制1115361),ADC数据有跳动。CH2SEL寄存器设置为0x11,一倍增益,通道2正负极内部短路的情况下,输出数据为591851(十进制),ADC数据有跳动,短接的情况下,输出的转换结果不应该是很小的数值才对吗?十进制591851对应的电平约为0.1707V,也不是参考电平,请问这种情况下,该如何确认问题,如何改进,附图如下: