Part Number: TLV5638
TI工程师您好,
我希望使用TI公司TLV5638_12bDAC进行VGA(压控放大器)的控制,在实测中使用了通道A快速模式,同时刷新Buffer,但是输出电压上调一瞬间后便归零,是否有使用TLV5638输出稳定确定直流信号的方法?
非常感谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TLV5638
TI工程师您好,
我希望使用TI公司TLV5638_12bDAC进行VGA(压控放大器)的控制,在实测中使用了通道A快速模式,同时刷新Buffer,但是输出电压上调一瞬间后便归零,是否有使用TLV5638输出稳定确定直流信号的方法?
非常感谢
您好,TLV5638是一款比较老的DAC器件,暂时没有相关使用它控制VGA的案例。所以针对您的问题,您可以将您的电路附上,在VGA的控制中,针对测试的增益,都是输出上调一瞬间就归零还是说特定增益下,输出不稳定?
我需要在我刷新后5638输出一稳定电压,直到我再次刷新这个电压值再改变即可,是否可以做到这种功能?
现在的问题是我刷新后5638有电压输出,但我刷新停止时输出便下降为0了,我想知道5638是否有输出电压保持功能
您好,这款DAC也比较老了,我看了下这款器件的数据手册,写完数据到通道A之后并且刷新buffer后,再配置R1R0=11将数据写入控制寄存器后,验证是否能得到稳定输出?