This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1298: 我们自己做的板子DSP与ADS1298通信存在问题

Part Number: ADS1298


亲爱的TI官方:

        我最近在开发DSP5535+ADS1298的应用开发。在开发过程中我遇到了一个问题。我们的自己做的DSP板与AD1298的通信一直未成功,具体问题的描述如下:
        1. 我们自己做板子飞线与ADS1298的开发板来进行通信能够成功,能够成功配置寄存器,读取设备的ID。我用逻辑分析仪抓到的信号如下所示,红色的是我抓取到了ADS1298的设备ID:0x92.

        2. 我们自己做的板子与板上的ADS1298通信一直未成功。信号0是CS,信号1是CLK,信号2是MOSI,信号3是MISO,不知道为什么,我DSP发送的SPI时序都是一样的,为什么我自己板子上的ADS1298就一直通信不成功呢?而且这个MISO引脚好像一直一直跟CS引脚保持一样的电平,没有有效的数据一样。

下面是我们板子上的ADS1298部分的原理图,情况紧急,能尽快帮忙分析一下这个情况吗?非常感谢!!

  • 您好,

    确认下,电路图中AGND与GND是否共电位?

    检查下,主从的通信电平是否兼容?

    您测试了几块板子是这种情况?是否可以多测几块板子,以排除这块板子硬件存在问题?