Part Number: ADS1292R
Other Parts Discussed in Thread: ADS1293EVM, ADS1293
您好!
我在用ADS1292R获取肌电信号的调试过程中,遇到一些问题,目前状况为:
1、可以正常测得内部1mv@1Hz的方波信号,如下图所示
2、Vrefp = 2.425V Vcap1 = 1.2V Vcap2=4.98V VRLDOUT= 2.92V,此时RLD_SENS=0x2C(如果RLD_SENS=0x20,VRLDOUT=1.485V,约为AVDD/2,但是RLD_SENS设置为0x20,RLDOUT是否可以正常用作人体参考及抑制共模干扰?)。
3、只用CH2,CH1设置为powedown模式,将CH2SEL的MUX2[3:0]设置为0x01,adc输出结果如下图2所示,但是如果MUX2[3:0]设置为0x00,在外部短接CH2P和CH2N的话,测试结果输出如下图3,明显差别很大。
4、如果MUX2[3:0]设置为0x00,在外部不短接CH2p和CH2N,那么输出结果如下图4所示,明显不太对,空闲状态下,正确的输出应该是一条略有抖动的直线才对。
初步判断可能是AGND和GND的连接问题,由数字电路引入了过多的噪声,没抑制下来,请问11.1.1.2章节(如下图5所示)的描述该如何理解及实现。
5、规格书里面11.2章节(下图6)的layout example 图示是否器件下方的红色框内不用铺地,只需要将AVSS和DGND用一条线连接起来?请问AGND和GND的0R连接点放在哪里比较好