This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8688A: 转换故障,一直输出固定值

Part Number: ADS8688A
Other Parts Discussed in Thread: ADS8688

  ADC _ 03_ADC2.pdf

各位大佬好:

我在使用ADS8688时,正常情况能正确读取寄存器值和AD转换数据。

但是有一定概率上电后出现:AD采集转换数据无论是自动扫描模式还是手动模式都一直维持一个错误数据,且8个通道,每个通道读取的值都一样。此时ADS8688程序配置寄存器能正确写入、读取(SPI通信应该没问题)。

1、给ADS8688的5V(CPU不断电)重新上电能解决该问题。

2、CPU重新上下电而ADS8688不断电,故障不能解除。

3.  通过SPI唤醒ADS8688也没有作用。

请问是否是ADS8688的内部出了问题,芯片没有正常工作,(配置寄存器能工作,而数据采集转换部分没有正常工作)
  • 您好,失效率高吗?下面几个方面需要验证下:

    DRDY stop后,可以读取所有寄存器的值,来确认这些寄存器的配置是否还都是正确的?

    监测Allarm引脚的状态,读取一下寄存器10h:ALARM Overview Tripped-Flag Register

    SCK是否稳定?

    REFIO和REFCAP电压正常吗?