This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,请问:
1. headroom是否指的无法输出到gnd的0V,比如在Iout是5mA的时候,最低输出只能到0.15V?
2. 如果问题1的回答为是,请问芯片DAC60508,如果Iout控制在0.5mA,headroom的值是多少呢?
谢谢
您好,
1.您的理解是对的,也就是举例电源轨的电压差。 比如参考下图,当(-5 mA ≤ IOUT ≤ 5 mA)时,无法输出0V,最低为0.15V. 同样也无法到达VDD,最高只能到达VDD-0.15V。
2. 参考FIgure33,headroom VS Iout的曲线,可以看到,大概在Iout为2.5mA的时候,deltaVout曲线才开始上升,之前几乎都是在0附近,所以0.5mA的话,应该是轨到轨,能达到VDD或者GND的。
您好,是的,理想情况下0 code对应的是0V,full code对应的是VDD。在任何代码中都将存在由总未调整误差 (TUE) 定义的偏差形成理想电压。 对于 DAC60508来说, TUE 为 0.1% FSR (最大值)。
所以5V满量程来说,误差为5V*1%=5mV. 可以说headroom为5mV。 得到的是5-5mV=4.995V。
我想针对这种极小电流,在曲线中无法衡量的基础上,可以根据TUE来评估。