This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS127L01: 量程达不到±VREF问题

Part Number: ADS127L01

根据Datasheet上说明,如果VREF=3V的话,量程应该在±3V

但在实际使用过程中,选用VLP mode,采样频率2k,出现信号幅度大约等于VREF/2的时候,高位2位出现反向,即00->11,11->00

  • 您好,

    也就是说,如果输入的电压是1.5V(VREF/2),1LSB=1.5522x10^-10,那么输出代码应该是4000 0012H,换成二进制是0100 0000 0000 0000 0000 0000 0001 0010,然后您实际输出是1000 0000 0000 0000 0000 0000 0001 0010 ?

    如果高2位都是0的话,输入电压应该小于1.5V,您可以输入一个恒定的1V电压信号,然后采集,看转换输出代码是什么样的吗?同时,用示波器测量SPI信号(SCLK 、CS 、DOUT、 DIN),看AD芯片实际输出是怎样的?

x 出现错误。请重试或与管理员联系。