Other Parts Discussed in Thread: ADS1118
我用ADS1118转换热电阻电桥信号,大概0.3V左右的电压。使用的命令字为0x058B,其他的0x048B,0x058A,0x058E都用过,但是转换的数值不断变化,没有稳定的数值。并且UCTXIFG总是1,无法变成0.读出的数值随机变化,请高手帮帮忙,十分感谢。
#include "msp430x54xA.h"
void GPIO_Init(void);
void SPI_Init(void);
void ADS_Config(void);
int ADS_Read(void);
signed int WriteSPI(unsigned int Config, unsigned char mode);
void main(void)
{
volatile int ADC_Result;
WDTCTL = WDTPW+WDTHOLD; // Stop watchdog timer
GPIO_Init();
SPI_Init();
ADS_Config();
while(1)
{
ADC_Result = 2*ADS_Read(); // Read data from ADS1118
if(ADC_Result>100) P5OUT &= ~BIT0;
else P5OUT |= BIT0;
//P1OUT = P1OUT;
}
}
void GPIO_Init(void)
{
//P1.0 CS
//P3.4 DataOut(SIMO)
//P3.5 DataIn(SOMI)
//P3.0 Serial Clock Out
P1OUT |= BIT0; //P1.0输出1
P1DIR |= BIT0; //P1.0设置为输出
P3SEL |= BIT0+BIT4+BIT5; // P3.0,4,5设置为第二功能
}
void SPI_Init(void)
{
UCA0CTL1 |= UCSWRST; // **Put state machine in reset**
UCA0CTL0 |= UCMST+UCSYNC+UCCKPH+UCMSB; // 3-pin, 8-bit SPI master
// Clock polarity high, MSB
UCA0CTL1 |= UCSSEL_2; // SMCLK
UCA0BR0 = 200; // /2
UCA0BR1 = 1; //
UCA0CTL1 &= ~UCSWRST; // **Initialize USCI state machine**
__delay_cycles(100); // Wait for slave to initialize
}
void ADS_Config(void)
{
signed int Config_Value;
Config_Value = 0x058B; // Initial Config Register
// ADS1118 configuration AIN0/AIN1, FS=+/-2.048, DR=128sps, PULLUP on DOUT
P1OUT &=~ BIT0; // Set CS low
WriteSPI(Config_Value,0); // Write configuration to ADS1118
P1OUT |= BIT0; // Set CS high
}
int ADS_Read(void)
{
unsigned int Data, Config_Value;
Config_Value = 0x058B;
// ADS1118 configuration AIN0/AIN1, FS=+/-2.048, DR=128sps, PULLUP on DOUT
P1OUT &=~ BIT0; // Set CS low
Data = WriteSPI(Config_Value,1); // Read data from ADS1118
P1OUT |= BIT0; // Set CS high
return Data;
}
/*
* Mode 0: Only write config register to ADS1118
* Mode 1: Write config register to ADS1118 as well as read data from ADS1118
*/
signed int WriteSPI(unsigned int config, unsigned char mode)
{
unsigned int temp;
signed int msb;
volatile signed int dummy;
//change the polarity of UCI0B_CLK to driver ADS1118.
UCB0CTL1 |= UCSWRST;
UCB0CTL0 = UCMSB + UCMST + UCMODE_0 + UCSYNC;
UCB0CTL1 &= ~UCSWRST;
temp = config;
if (mode==1) temp = config | 0x8000;
while(!(UCA0IFG&UCTXIFG));
UCA0TXBUF = (temp >> 8 ); // Write MSB of Config
while(!(UCA0IFG&UCRXIFG));
msb = UCA0RXBUF; // Read MSB of Data
while(!(UCA0IFG&UCTXIFG));
UCA0TXBUF = (temp & 0xff); // Write LSB of Config
while(!(UCA0IFG&UCRXIFG));
msb = (msb << 8) | UCA0RXBUF; // Read LSB of Data
while(!(UCA0IFG&UCTXIFG));
UCA0TXBUF = (temp >> 8 ); // Write MSB of Config
while(!(UCA0IFG&UCRXIFG));
dummy = UCA0RXBUF; // Read MSB of Config
while(!(UCA0IFG&UCTXIFG));
UCA0TXBUF = (temp & 0xff); // Write LSB of Config
while(!(UCA0IFG&UCRXIFG));
dummy = UCA0RXBUF; // Read LSB of Config
while(UCBUSY&UCA0STAT);
//change the polarity of UCI0B_CLK to driver ADS1118.
UCB0CTL1 |= UCSWRST;
UCB0CTL0 = UCMSB + UCMST + UCMODE_0 + UCSYNC;
UCB0CTL1 &= ~UCSWRST;
__delay_cycles(10);
return msb;
}