Part Number: ADS131A04
Other Parts Discussed in Thread: THS4521
请问ADS131A04器件在+5V单模拟电源,全差分输入,使用外部基准时规格书允许的最大基准电压是AVDD-0.5V,个人理解这个0.5V是受限于内部基准缓冲器的摆幅限制,这种情况下,如果使用5V的外部基准,电流会不会流入缓冲器导致故障.
差分驱动器是THS4521,最终ADC输入信号的范围大约正负4.8V
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
使用外部基准的话,需要从REFXT输入基准电压,因为REFXT管脚内部集成有buffer以增加输入阻抗;REFP是buffer的输出管脚,如果在REFP输出端加5V电压,有可能会损坏buffer,因为内部集成buffer输出端口的耐压datasheet没有给出。
外部基准时规格书允许的最大基准电压是AVDD-0.5V,这个0.5V应该是受限于内部基准缓冲器的摆幅限制;但是客户从REFP外接5V电压,没有经过内部集成的buffer,还需考虑外加buffer以增加输入阻抗(这是考虑REFP管脚能够承受5V电压的前提下的说法)
REFEXT管脚加5V电压不会损坏,可以承受的住,因为REFEXT的绝对最大额定值是AVDD + 0.3V。但是仅允许加AVDD – 0.5V,超过这个范围,那么ADC datasheet中的性能不能保证。



差分驱动器是THS4521,最终ADC输入信号的范围大约正负4.8V
您可以考虑使用前端电路将ADC的输入范围缩小一倍,即缩小至±2.4V。这样就满足AD的输入范围了。