ADS1283采集数据时,发现数据延迟参数不太正确。手册给出了群延迟参数是31个DRDY信号,我的采集读取数据也是在31个DRDY信号后,但是采集的数据起始部分缺少了31个点的信号。我是采集GPS的PPS信号作为基准信号,当采用31个DRDY参数作为延迟输出时,不同的采样率(250-4KSPS)下总会在起始时刻出现31个左右的点是非正常数据。之后的数据都是根据PPS边沿对齐整数秒时间的。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
整体信号就延迟采集了31个DRDY信号,怎么才能保证0时刻既不出现非正常数据,又能保证数据不延迟后才输出呢?
这个应该是没有办法的,因为如前面所述,其Settling time为62个DRDY信号。
您帖子中说“之后的数据都是根据PPS边沿对齐整数秒时间的。”,这里有描述说“我之前把31这个参数改为62个之后确实没有了非正常数据,但是读取数据就不是0时刻对齐PPS信号了”,那么,您这里可以把0时刻定义为62个DRDY信号之后的第一个数据,即将0时刻再延迟31个DRDY信号