TI的FAE工程师,您好,最近在使用ADS830,由于系统是单电源,所以我按照其手册推荐的电路来搭建,即datasheet中第8页,OPA681作输入端前的同相放大器的电路。运放我由于手中没有OPA681,所以用同是电流反馈型运放的OPA691来代替(应该没有问题吧,压摆率和带宽都是符合我系统的要求的),实测中发现,OPA691的同相输入端的电压是2.46V,这个电压取自ADS830的参考引脚REFT和REFB, 与标准值相差不大,可以接受。但是,当输入信号后,发现同相输入端的前面存在一个高通滤波器,在电容是0.1uF,REFT和REFB所接出电阻是1k时,截止频率是3.2k Hz,由此我认为是两个1k并联后是500欧,与0.1uF电容组成高通滤波器,理论计算值与实际是相符的。所以,由于我输入信号是低至5Hz的交流信号。所以,我想通过加大电阻和电容值来减小此滤波器的截止频率,于是,我把电容改为10uF,1k电阻改为33k, 如此截止频率就很小了。然而,实际测量结果却是700Hz的截止频率。我不懂了。我再把33k电阻换成100k, 截止频率居然变成了5k多了。这是什么情况?难道我想错了吗?希望可以得到您的指导。谢谢。