Other Parts Discussed in Thread: TMS320F2812, ADS1282, ADS1283, ADCPRO, ADS1281
ADS1282是不是没有片选信号,想用一个TMS320F2812挂2片ADS1282,是否可行?有什么需要注意的问题么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
谢谢您,我的邮箱是caix08@mails.tsinghua.edu.cn。
现在我的硬件板子已经做出来了,使用2812的SPI带两块ADS1282芯片,还有一个时钟芯片、一个SD卡,也是利用SPI接口来传输数据。本来是打算用两个IO引脚分别控制芯片的pdwn引脚,但是发现这样数据率太低了,无法实现1KHZ的采样。
现在还是想在现有的硬件电路上进行程序开发,您说的加缓冲或者采用ADS1283估计要等到下一步再去做。
现在有如下两个方案:
1、采用modulator output mode ,利用M0、M1和MCLK来输出数据,这样就可以腾出SPI口给其它设备用。
2、利用sync来控制两个芯片,这样数据率会高一些。但是,SPI口还是会被占用,不能使用其他设备。
不知道我这两种方案哪一种更加可行一些?如果都不行,就只能更改硬件电路了。
ADS1283的资料能否给我一下,我们有用过ADS1281,我的邮箱是eiate@163.com ,谢谢!