通道0~7设置采集范围为0~5V,通道0~7在无输入信号的情况下,通道0~6转换值为0、通道7转换值为3770(0.294V).输入信号源电压值低于1V时,各通道的转换值与无输入信号相同。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
通道0~7设置采集范围为0~5V,通道0~7在无输入信号的情况下,通道0~6转换值为0、通道7转换值为3770(0.294V).输入信号源电压值低于1V时,各通道的转换值与无输入信号相同。
很高兴您之前的问题解决了,感谢您的反馈;
输入引脚悬空,会存在一定的输出,因为悬空的管脚会耦合空气中的电磁干扰。因此,模拟输入端一般都是不能悬空的。对于ADS8688,您可以通过寄存器控制关断这个不需要的通道。如果您要检测输入是否悬空,您可以参考下面文档:
https://www.ti.com.cn/cn/lit/an/zhcaas8/zhcaas8.pdf
悬空的那个电压不是ADS8688芯片内部的偏置电压吗?
您是指下图中的VBn 电压吗?
不是的。ADS8688采集的是 (AIN_nP – AIN_nGND)两端的电压,在AIN_nP悬空时,那么它的电压就是耦合的空气中的电磁干扰形成的电压,这个是不确定值,因此此时ADS8688的输出是不确定的。
我想要实现的功能是8个通道能同时使用并且在我不接入信号的时候我得到的转换值为0.
这应该无法直接实现。内部集成的PGA是一个全差分放大电路,如果想要在AIN_nP悬空时,采集的转换值为0,那么需要在这个管脚上接个对地的开关,无输入时通过开关接地,有输入时断开开关正常采集输入电压。