Part Number: ADS1299

你好,这是我想实现用来测脑电的方案配置,没有使用右腿驱动也没有SRB1或SRB2,也没有使用菊花链。我使用的是整个ADS1299套件,目前能正确的读取ID寄存器,但后面读出的数据一直是7FFFFF或800000,请问我的寄存器应该如何配置呢,希望可以得到你的帮助,谢谢!

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS1299

你好,这是我想实现用来测脑电的方案配置,没有使用右腿驱动也没有SRB1或SRB2,也没有使用菊花链。我使用的是整个ADS1299套件,目前能正确的读取ID寄存器,但后面读出的数据一直是7FFFFF或800000,请问我的寄存器应该如何配置呢,希望可以得到你的帮助,谢谢!

如何将输出代码转换为输入电压,您可以参看下面链接FAQ:
https://e2echina.ti.com/support/data-converters/f/data-converters-forum/192643/faq-ads129x
您将MUXn[2:0] 设置为001 : Input shorted (for offset or noise measurements),看转换结果是多少?
配置CONFIG2= D0h,基准电压4.5V的话,输出应该是+-1.875mV的方波;
负为187mV,而正的是0.025uV,这个结果是不正确的,通过上面FAQ链接看下是否转换过程出错?或者您可以附上您读取的code吗?我手工转换下,以验证采集数据是否正确
非常感谢你的耐心解答,我之前的转换是错误的,现在未转换时,方波测试基本为2400(底部)、16772667(顶部)。因为CONFIG2= D0h、CHnSET=05h。按照我现在的理解,LSB=4.5V16777215=0.2682μv? 那么2400x0.2682=643.68μv=0.64368mv? 16772667=> (16772667-16777216)x0.2682=-4549x0.2682=-1.2200418mv?
同时通道2我设置为CHnSET=01h时,进行短接噪声测试,输出基本都是16776015约为-0.3mv?,则为以上我是否有理解错误的地方,期待得到您的回复,这对我帮助很大,非常感谢
上面计算过程没有错;但是输出结果是不正确的,您用示波器查看基准电压和供电电压是否稳定?
如果基准电压和供电电压没有问题,您可以附上您读取采集数据的SPI时序图吗?将SPI信号显示在同一屏幕中,我看下时序是否正确。