This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC7718: 这是原理图的问题还是代码的问题

Part Number: DAC7718


    请问一下我这个原理图画的有问题吗,我需要DAC单极性输出,输出电压范围在0-16V。AVDD供电32V,DVDD和IOVDD输入5V,参考电压VREF输入5F。寄存器采用默认,根据电压公式计算,OFFSET-B与AGND-A连接,OFFSET-A与AGND-B相连接。OFFSETDAC_CODE=0,控制输入INPUT_CODE为0X7780,应该输出14V.但是我代码设置好后,用32单片机开控制,发现输出电压不是14V而是24V,并且电压会跳变。我想知道这是原理图的问题还是代码的问题。我一直找不到问题在哪。