Other Parts Discussed in Thread: DAC5687
最近正在试用Dac5687,测试发现杂波性能还可以,谐波分量却很大,而且不止有二次三次谐波,一直到十次输出频率处谐波能量都很大,大约有-40dB左右。
输出端电路严格按照datasheet的推荐选用1:1射频变压器,初级正负端分别上下拉50欧电阻,中间跨接100欧电阻,负载50欧。自己也计算过,匹配确实没有问题。测试时,只在控制寄存器config0中选择mode X2,config2 中Bit nco 置0,并把控制Bit bpfmix 置1,结果确实得到了单载波,杂波性能不错,谐波却不尽人意。不但谐波能量大,分量多,而且频谱中其能量不稳定,一直在抖动,因为5687的功能较多,控制也比较复杂,不知是不是里面的那个功能模块对谐波有影响??如何关掉或避免??还是此款IC单载波输出时,这样是正常的?
补充一点,在5687的手册中没有找到相关的谐波指标,所以无法对比。而且高次谐波分量相比二次三次谐波也无衰减,Pcb上其余无关电路以全部powerdown,应该无影响,Dac输入数据由FPGA产生,除时钟外再无其他高频信号。
测试条件:mode X2,采样时钟250MHz,输出频率5MHz,外部时钟模式,由clk2提供Dac工作钟