我通过spi对ADC12DL3200进行寄存器配置,但是当寄存器0x200的值为0x00时VIVADO ila 抓取到ADC的采样数据,当0x200的值为0x01时没有数据。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我通过spi对ADC12DL3200进行寄存器配置,但是当寄存器0x200的值为0x00时VIVADO ila 抓取到ADC的采样数据,当0x200的值为0x01时没有数据。
您是否验证了可以正确写入和读出寄存器值?因为LVDS_EN=0时,LVDS接口块是保持在复位状态的,输出是powered down 的,不应该有输出。
设置 CAL_EN = 1后,设置LVDS_EN=1,您用示波器量LVDS接口有数据输出吗?因为我想排除下VIVADO ila的影响,数据手册明确说明LVDS_EN=0时,输出是powered down 的