This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS5271: ADS5271的VCM控制问题

Part Number: ADS5271

ADS5271的VCM输出是怎样控制的?我前端有个差分放大器,ADS5271接前端运放的VCM,上电后ADS5271的VCM会输出3V,程序加载ADC打开后,VCM输出正常1.45V;但把VCM 与差分放大器的VCM断开,他的输出是1V;如果是把ADS5271的输入与前端运放的输出断开,ADC的VCM的输出0V;

  • 这个主要是运放的输出到ADC的输入,输入与VCM相连接,然后VCM输出又给运放增加了共模偏置,这样运放输出的共模就是3V,想请教这个运放输出只能做交流耦合,不能做直流耦合?

  • 您好,

    您的意思是前级运放的输出信号共模电压是3V?

    可以直流耦合,但是要设置输入信号的共模电压在1.45V。

    但把VCM 与差分放大器的VCM断开,他的输出是1V

    您这里是直流耦合,前级输入模拟信号的共模电压不是1.45V,那么可能是这里造成其输出共模电压异常为1V,而不是正常的1.45V。

    如果是把ADS5271的输入与前端运放的输出断开,ADC的VCM的输出0V;

    这里测试时,VCM是否还与前级运放的VCM是连接状态?如果还是连接状态,可能是运放的VCM拉低了ADC的VCM。

  • 非常感谢!但是我想请教一下几个问题。

    1、我想知道ADS5271的VCM输出 buffer是通过什么来控制的?因为ADC后端的FPGA上电完成后,ADC的VCM输出是正常的1.45V;

    2、上电后ADC未打开时,由于ADC的输入与内部 VCM相连接,ADC的输入共模为3V,因此ADC的VCM输出是3V,ADC的VCM与前端运放的VCM相连接,因此前端运放的输出共模就是3V,所以就形成了一个环路;所以我猜测ADC未打开时VCM按正常是0V,但现在是3V是因为前端运放输出共模就是3V,因此我验证断开前端运放的输出,ADC的输出就是0V;这说明是互相影响,有什么办法阻断这个共模3V的输出?

    3、上电后ADC未打开时VCM就是3V, ADC打开时VCM输出是正常1.45V,我担心板卡上电后,ADC还未打开时VCM是3V,这时外部又有信号灌入,这时ADC的输入会超过其输入范围,可能损坏ADC;

  • 1、VCM电压是REFT和REFB的中间电平,具体见数据表“REFERENCE CIRCUIT DESIGN”部分:

    2、ADC未打开是指PD是高电平吗?PD高电平时,VCM是三态状态,被弱下拉至地,是0V。

    如果PD高电平时,ADC的模拟输入信号共模为3V,直流耦合,那么可能会造成ADC的VCM输出是3V,如下输入电路:

    3、我想只能通过其他电路产生前级运放的VCM了,因为ADC如果是PD状态,其VCM就是由其输入电路决定的,不能调节输出共模电压为1.45V。

  • 非常感谢!VCM buffer 的控制就是和手册上一致的跟PD状态决定的