This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1282: 输出位数和数据问题

Part Number: ADS1282


请问同时使用ADS1282的两个差分通道进行采集,采用RDATA来通过命令读取数据,那么是会同时输出AIN1和AIN2的数据吗?输出顺序是什么样的呢?

另外,ADS1282的32位和24位输出应该怎么设置呢?

谢谢。

  • 您好,

    ADS1282不是同步转换ADC,因为它只有一路ΔΣADC,它是通过多路复用器MUX实现的多通道输入。因此,它是通过寄存器 CONFIG1 MUX[2:0]位选择输入通道的,它不能同时输出AIN1和AIN2的数据。

    另外,ADS1282的32位和24位输出应该怎么设置呢?

    在发送24个SCLK脉冲后停止发送SCLK来实现的,然后等待下一个数据的DRDY信号。或者说仅读取输出数据的高24位。