This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS127L01: 这款ADC的指令寄存器的问题

Part Number: ADS127L01


 1、ADS127L01这款ADC的供电引脚Pin1-LVDD分为1、INTLDO=0时是供电输出功能,2、INLDO=1时是外部输入1.8V。配置成输出或者输入有什么影响吗,是影响功耗吗?

2、这款ADC是不是不能通过指令的形式配置ADC的工作模式,只能读取当前的工作模式,一旦硬件上配置好模式,就不能更改,除非改硬件。是这样吗?

3、但是指令可以发“STOP”和“START”命令,这样就可以不用引脚“START”来控制。是否?

  • 您好,

    1、是的,主要是功耗考虑,如果功耗允许的话,可以使用片上LDO以节省外部供电芯片和PCBLayout空间。

    2、您是指下面蓝色部分的工作模式吗?如下蓝色部分所述,可以通过微控制器或 DSP的 I/O 来设置这些管脚的状态,请注意,通电后,当在硬件模式引脚上检测到变化时,ADC会自动发出重置。为确保同步,需发出软件复位命令,或在模式更改延迟td(MD)后脉冲复位/PWDN引脚。

    3、是的。