我在ADS127L11datasheet的9.2.1节“ Design Requirements”,手册举了个设计案列,将输入信号在Fmod频率12.8Mhz附近衰减90dB,90dB时电压增益=0.0000316,已经非常小了。我的问题有2个。
1、该例子是考虑在什么样的应用下要衰减到90dB,衰减到45dB不行吗?-45dB时电压增益=0.00562,也很小了。
2、
画线部分是怎么理解呢?为什么说这个滤波器的“rolloff”是“关键功能”
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我在ADS127L11datasheet的9.2.1节“ Design Requirements”,手册举了个设计案列,将输入信号在Fmod频率12.8Mhz附近衰减90dB,90dB时电压增益=0.0000316,已经非常小了。我的问题有2个。
1、该例子是考虑在什么样的应用下要衰减到90dB,衰减到45dB不行吗?-45dB时电压增益=0.00562,也很小了。
2、
画线部分是怎么理解呢?为什么说这个滤波器的“rolloff”是“关键功能”
您好,
1、抗混叠滤波器的作用是将 噪声信号的 振幅降低至 ADC 无法再检测到的水平,也就是说需要将其降低至小于1/2个 LSB的水平。具体衰减多少倍是与噪声信号或者说混叠信号的峰峰值有关,通过衰减一定的倍数使其小于1/2个 LSB,这样才不会对采集的有效信号产生影响。
2、不是说“滤波器的“rolloff”是“关键功能””,而是说设计的滤波器在fMOD 频率处的rolloff(滚降)或者说衰减斜率是关键,滤波器衰减斜率越陡效果越好。因为设计要求是The goal of this design is an antialias filter at the ADC input to attenuate out-of-band signals at the modulator sample rate (fMOD). The requirement of the antialias filter is 90-dB attenuation at the critical fMOD frequency (12.8 MHz in high-speed mode)