我们最近在使用ADS114S08做T型热电偶的检测,参考使用内部2.5V,PGA 为128倍,在室温情况下,我们发现检测出的温度时不时会升倒最大值,或者最小值.然后我们观察状态寄存器,发现温度检测有问题的时候,以下几个状态可能会出现.

因为端子上只有热电偶,按照这些状态的字面解释,就是PGA输出电压过高或者过低了,热电偶的电压只有mV级别,就算128倍放大,也到不了电源轨和地轨。
下面是外围原理图,每个芯片用5对差分,一对差分采PT1000,四对差分采热电偶电压

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我们最近在使用ADS114S08做T型热电偶的检测,参考使用内部2.5V,PGA 为128倍,在室温情况下,我们发现检测出的温度时不时会升倒最大值,或者最小值.然后我们观察状态寄存器,发现温度检测有问题的时候,以下几个状态可能会出现.

因为端子上只有热电偶,按照这些状态的字面解释,就是PGA输出电压过高或者过低了,热电偶的电压只有mV级别,就算128倍放大,也到不了电源轨和地轨。
下面是外围原理图,每个芯片用5对差分,一对差分采PT1000,四对差分采热电偶电压

您好,状态寄存器的值这几位都读取的是1是吗?bit7 FL_POR读取的是什么值?
另外,上电时序是否满足Figure 83. Power-On Reset Timing Sequence?
您好,首先ADS114S08虽然是多路输入,但是输入前端集成了多路复用器,所以我想和您确认下是切换到哪路输入报错的?四对热电偶输入是否都有尝试切换,结果是一样的吗?
另外,thermal pad是否有铺铜接GND处理?
其次,PGA增益是否有尝试降低,看下是否还报错呢?
这里有一篇应用手册可以参考下,其中对电路设计,PGA增益和激励电流源的选择都做了介绍:
您好,您的意思是连接热电偶的输入端悬空了,输入前端的MUX 选择了其他输入,此时这个通道采集到的值不稳定是吗?
这是因为,悬空的输入有可能浮动到电源范围内的任何电压值,有时ESD或者其他部件内都会存在漏电流,可能会将输入电压拉到其他电压值,没有固定的偏置电压,所以您可以将其接到1/2Vcc 或者接地。